Part Number: ADS1256
Hi,
My customer is using the ADS1256 with the REF5025 external reference on a DAQ demo board. He had issues with noise associated with the device at a full scale differential input of 4V, and the customer was looking for an ADC capable of <50uVp-p over a 600Hz input bandwidth.
Based on the REF5025 datasheet spec, the customer believes the reference noise would be 3uVp-p*2.5=7.5uVp-p over a 0.1-10Hz bandwidth. Ignoring 1/f noise, this would be equal to 158nV/rtHz. Now, over a 600Hz bandwidth this would be 23uVp-p. Based on these calculations, the customer believes the demo board should be <50uVp-p at 4V input and 600Hz.
Can you confirm? Do you know if the customer can reach these spec with the ADC and Ref he has, or do you recommend another part?
Regards,
RP