This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8775: DAC8775 power supply

Part Number: DAC8775

Hi team,

 

In the DAC8775 datasheet figure 137, the power supply recommended with external supplies is +12V. But upper in the document, the minimal voltage is +12V.

We have on our design a power supply of +12V +/-3%.

Can we power the DAC with +12V +/-3% without problem? Or under +12V the DAC lose some accuracy?

 

Thanks for your help.

Best Regards.

Olivier

  • Hi Olivier,

    The device will likely function below the recommended minimum input voltage but the specifications listed in the datasheet can only be guaranteed if the input voltage is between the recommended min and max. I would suggest using a supply set slightly above the minimum input voltage to avoid this condition.

    Thanks,
    Garrett