Other Parts Discussed in Thread: ADS1118
HI
i face the problem where ADS1118 returns to Arduino/STM32duino unexpected hiigh values like below. AIN lines are connected to ground via 10k. Same when i put a signal into in i.e. 1V (i choose 1024mV amplify).
i tested 32 and 16 bit mode as well. Unfortunetelly with same results. I also tested different delayes when CS goes low etc. I use 860SP but tested also other modes - same bad results.
Below also SPI interface. i can not find corelation why it suddenly sends high score - i checked previous frames and all are fine. I checked this on two microcontrolers and always the same. I power the ADS1118 supply from 3,3V or 5V. I use also LC filter to clean voltage, I tested SPI speed from 500kHz up to 4MHz. I used serial 150ohm rezistors and same.
Please give me some hint what is wrong.
Thanks in advance
Tom