Part Number: TSW14J56EVM
Hi
I am running the HSDC Pro v4.9 in my Win 10 laptop with a TSW14J56 EVM. It takes about 2 min to detect the board itself. I was wondering if there is any specific reason this might happen?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSW14J56EVM
Hi
I am running the HSDC Pro v4.9 in my Win 10 laptop with a TSW14J56 EVM. It takes about 2 min to detect the board itself. I was wondering if there is any specific reason this might happen?
Yes. I have a Windows 7 laptop as well. It takes like 2 seconds in it. Hence my question.
Do you have any updates on this issue. Not that it limits my working with the board in anyways, but its inconvenient having to to wait that long every time I connect the board whereas in Win 7 it connects in no time.
Aravind,
Can you try manually uninstalling the Cypress USB3.0 drivers then uninstall HSDC Pro GUI, then re-install HSDC Pro. Also, make sure you are not using any type of USB hubs. These have been know to cause issues wit this interface. What type of machine are you using? Does it have a USB3.0 port? If so, have you tried this port?
Regards,
Jim