I'd like to measure the amplitude of an amplitude-modulated 4V p-p 100kHz sine wave, at 18-20 bits resolution. I could
1. Demodulate it to a 2V p-p rectified sine wave, lowpass filter, amplify, and sample at 200ksps, or
2. Sample synchronously at the peaks, at 200ksps, and demodulate digitally
Which is lower noise? 2) is simpler and would not have 1/f noise, but would total noise be lower?
Thanks!