Part Number: AFE4490SPO2EVM
Other Parts Discussed in Thread: AFE4490
Hello,
I have a question regarding the averaging mechanism of the AFE4490.
I see that the maximum number of averages is 16 and that the equation for averages is given by: (0.25 * PRP / 50us) -1.
This makes sense to me if the duty cycle is 25%. However, if the duty cycle is less than 25%, should the 0.25 in the equation above be changed to the value of the new duty cycle?
The GUI allows me to set the number of averages given by the equation, even if it should be too many averages given the shorter duty cycle. Does this mean that the "extra" averages are insignificant?
Say a 5% duty cycle should correspond to 4 averages max, if I use 0.05 rather than 0.25 in the equation. If I set the number of averages to 16 anyway, are the extra 12 averages essentially ignored because the LED is only being sampled for ~200 microseconds? Or should including the full 16 averages improve my signal?
Thanks!