Part Number: ADS54J69
In the ADS54J69 datasheet, registers 39h, 3Ah, and 56h have bit fields labeled "PERF_MODE" but the field description tables do not actually describe what these PERF_MODE bits do. Also, step 3 of the suggested device initialization sequence is titled "Performance Modes", but only says to write 20h to address 59h. Can someone provide some explanation or guidance on the PERF_MODE bit values?