Other Parts Discussed in Thread: PGA460
Dear Akeem,
Many thanks
I confirmed a correct signal though I can't get the signal from 50cm to 150cm so that I changed the value of burst count from 0x01 to 0x0F in short mode so work is well
A range in short mode is from 15cm to 150cm but I can't get a distance of object as 15cm when returning 20cm
How can I get 15cm of distance? and if the burst count is increase, do I need to increase blanking timer ?
If I have to need, Please let me know a way of calculation
Wongeun