This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8363EVM: does this work with MMB3

Part Number: ADS8363EVM
Other Parts Discussed in Thread: ADS8363

I would like to know if the ADS8363EVM works with MMB3 or if there is another interface board that works with it?

  •  Hi Rhett,

    Unfortunately, the ADS8363EVM is released as a stand-alone board without a controller.  Therefore, there is no released EVM specific software or GUI associated with this evaluation board.

    However, it is possible to connect the evaluation board to one of the C2000 DSP experimenter kits.  The Application Report:  "Interfacing to the ADS8363 Pseudo-Differential Operating Mode" (SLAA633) discusses the interface connections and provides code snippets:

    http://www.ti.com/lit/an/slaa633/slaa633.pdf

    Thank you,

    Kind Regards,

    Luis