Part Number: TIPD158
Hello.
I find a mistake in the schematic for TIPD158 "Low-Cost Loop-Powered 4-20mA Transmitter, EMC/EMI Tested".
On page 25, Figure A-1 "Electrical Schematic", Appendix A, the Vreg should be 3V, not 5V (I assembled this circuit and measured).
Even on page 9, there is a comment "The loop regulator uses the TL431B programmable shunt regulator to provide a 3 V supply to the loop transmitter using the rectified supply voltage from the diode bridge. Figure 8 shows the loop regulator section of the design."
Kind Regards,
Pawel Szczurowski