This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900: DAC Vs current

Part Number: PGA900

As per the TI document  " PGA900 as a 4- to 20-mA Current Loop Transmitter " DAC code for 4mA is  2096 (DEC) and for 20 mA it is 10476 (DEC). Hence the total span in DAC code is 8380. But in my circuit DAC code span for 4 - 20 mA is only 8330. Details of characterization of my circuit as follows. Current measured using Keithley 2000 multimeter.

DAC code (HEX)    DAC code (DEC)    4-20 mA loop current
818                                2072                           4.0036
a24                                2596                           5.008
c29                                3113                           6.004
e30                               3632                            7.0009
1033                            4147                             8.0009
144c                            5196                             10.005
28a2                            10402                           20.000