Part Number: LDC2114EVM
Hello,
I have a problem during instalation "Sensing solutions GUI-1.9.4" on win 7 64bit.
The problem is that no driver instaled for LDC2114EVM.
I need driver for win7 for LDC2114EVM.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LDC2114EVM
Hello,
I have a problem during instalation "Sensing solutions GUI-1.9.4" on win 7 64bit.
The problem is that no driver instaled for LDC2114EVM.
I need driver for win7 for LDC2114EVM.
Thank you.
Hi Jan,
First, please go to Device Manager and check under the COM ports section whether you see "EVM" when the board is connected to the PC.
If it is not listed, then you may need to manually force the Device Manager to look for a driver for the connected device in the GUI installation folder which is usually C-> ti -> Sensing Solutions EVM GUI 1.9.4 -> EVM Driver
If that was not the issue, then you may need to try running the GUI in Windows Compatibility Mode. You can try Windows 7 or Windows XP (Serivce Pack 3) compatibility modes. You may also need to restart your PC after installing the GUI.
Regards,