Hello I am trying to calculate a given Vout for a known B field and two different values of Rshunt, my parameters are:
B = 0.05mT (0.5 Gauss)
Rshunt1 = 100 OHMS
Rshunt2 = 330 OHMS
Can you please help me with this calculation.
Thanks
-E
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello I am trying to calculate a given Vout for a known B field and two different values of Rshunt, my parameters are:
B = 0.05mT (0.5 Gauss)
Rshunt1 = 100 OHMS
Rshunt2 = 330 OHMS
Can you please help me with this calculation.
Thanks
-E
Hello Eduardo,
Thanks for using the forum to get answers to your questions.
In our DRV425 Tools & Software tab you can find a calculator that will help with this.(DRV425 System Parameter Calculator) The calculator will also help you see if you will have any design issues and other information. Please note the output is ± due to the fact the field can be positive or negative and the output is centered around Vref.
The calculation can also be done with Equation 1 of the data sheet.
Vout = B × G × Rshunt × Gamp
B= 0.05mT (or other field to be measured)
G = 12.2mA/mT
Rshunt= 100Ω or 330Ω
Gamp = 4 V/V
Vout(100Ω, 0.05mT) = ±0.244 V +Vref
Vout(330Ω, 0.05mT) = ±0.805 V +Vref