Other Parts Discussed in Thread: DAC5687
I presently have six DAC5687 running at 96 mhz. with the nco commanded to 12 mhz all is well,as all spurs would fold back under. When i command 12.04Mhz the dacs have modulation at 11.06mhz apprx -83 db down which is no surprise. What I've seen is that if I re-run an labview application which resets, and commands the frequency, the spurs will sometimes drop to -90db. Any thoughts on how to achieve the -90db all the time, and what is actuall happening when i reset. Is it possible that the 90 degree delta from the sine/cosine generator has an slight inbalance, and sometimes I'm catching it at exactly 90 degree. I realize that -83 is good, but my customer has seen the -90db, and wants it.
Thanks,
Bill