Part Number: LDC1612
Hi,
We are looking for linear Displacement measurement sensor based on Inductive sensing technology.
Requirement is mentioned below.
1. Total traveled distance will be less than 100 um.
2. Resolution needed less than 1 um.
3. Maximum target diameter will be 20 mm.
4. Spacing between targets and coil is flexible.
Is it possible to measure such small displacemt of less than 100 um using Inductive sensing?
I read sub micron measurement is possible in LDC1612 datasheet.
Could you help me to understand the feasibility of this requirement using inductive sensing?
Thank you,
Regards,
Rajesh M