Hi Team,
I received the following LMP92066 questions and would like your suggestions regarding having the default output at -5V. What would you recommend? Regarding the programming tools and connections questions, I assume this is typically done by the system processor since it's just a set of I2C writes, and pull-ups can be in the processor if they are of similar strength, correct?:
We need advice and a full solution for EEPROM programming:
- What is the Burner tool do we need to use (software and also USB adapter)
- What is the connector we need to use in our circuit and what are the inputs and outputs from the LMP92066PWP we need to connect.
- How can we start the process with -5V and not 0V in order to avoid damaging the component that will be connected to the DAC output.
- What is the Right way to connect the LMP92066PWP to the FPGA/ARM in order to burn the EEPROM
- Do we need to put the I/O pins with Pull up like in the schematic or we can pull them up by the FPGA or by the USB burner.
Thanks,
Antonio