This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214: FDC2214 can be only use Capacitive Touch Sensor? No use proximity sensing

Part Number: FDC2214

FDC2214 can be  only use  Capacitive Touch Sensor? No use proximity sensing

  • Hi David,

    The FDC2214 is our highest resolution capacitive sensing device, and can be used for both proximity sensing applications and capacitive touch applications. Its resonance-based architecture makes it more noise immune than traditional switched-capacitor based architectures, which is desirable for proximity sensing applications. You can read more about using the FDC2x1y devices for proximity sensing in this app note

    Regards,