Dear Sir : I have a AFE4400EVM but with old firmware and could not connect with GUI V2.0. And the AFE4400EVMFWSRC-v1.4 could not be used to update to new v1.4 firmware. How could I update to new V1.4 firmware of the evm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir : I have a AFE4400EVM but with old firmware and could not connect with GUI V2.0. And the AFE4400EVMFWSRC-v1.4 could not be used to update to new v1.4 firmware. How could I update to new V1.4 firmware of the evm?
It did not work, the firmware on evm is too old and the update program(V1.2.1) did not recognize the evm. The old firmware's message communication protocol is not the same as v4.0. I need an update program with older message communication protocol.