This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8528: Power Supply Recommendations

Part Number: ADS8528


Dear Technical Support Team,

Ramp up of HVDD and HVSS  are small voltage(±3V) as long as 3ms on powerup. After supplied AVDD and DVDD completely,  HVDD and HVSS are supplied ±15V.

I guess that it is caused by ESD structure between AVDD  and HVDD  on datasheet.

Are the  IHVDD and IHVSS increasing until supplied both AVDD and DVDD?

【Datasheet】

ーーーーーーーーーーーーーーーーーーーーーーーーーー

The ADS85x8 require four separate supplies: an analog supply for the ADC (AVDD), the buffer I/O supply for the digital interface (DVDD), and the two high-voltage supplies driving the analog input circuitry (HVDD and HVSS). Generally, there are no specific requirements with regard to the power sequencing of the device. However, when HVDD is supplied before AVDD, the internal electrostatic discharge (ESD) structure conducts, increasing the IHVDD beyond the specified value until AVDD is applied.

ーーーーーーーーーーーーーーーーーーーーーーーーーー

Best Regards,

ttd

  • Hello,

    The ramp up on HVDD/HVSS cou'd also be due to the limits of the P24V source. It seems you are supplying all our power supplies of the device off the same source. All the supplies are bring brought up at the same time, this could be loading the source too much. What you using to supply the 20V on P24V?
    Could you try adding a delay, bring up AVDD/DVDD up first and then HVDD/HVSS?
    Also, you could try different sources for HVDD/HVSS and AVDD/DVDD?
    This would help eliminate any limitations on the source power supply
    Regards
    Cynthia