This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4222: Drive for ADS4222

Part Number: ADS4222
Other Parts Discussed in Thread: THS4511, , THS4509,

Hi,

  I want to drive ADS4222 in DC coupled mode using THS4511 amplifier. However, the common mode of the amplifier and ADS4222 are different. Please suggest proper circuit to drive the ADC with the amplifier.

The source signal to the amplifier is output of a unity gain stage(part of a detector) swinging from 0.9 to 1.8V. The input signal frequency is from DC to 10 MHz.

Regards,

Vishak