Part Number: FDC2214EVM
Other Parts Discussed in Thread: FDC1004EVM, , FDC2114, FDC1004, FDC2214
Hello,
I am using fdc1004evm and fdc2214evm for distance measurements and wanted to double check if I'm doing it correctly, since I have some noise issues)
Background:
Due to the nature of my applications, I need to use 1.5 m long coax cables to connect my 2''x2'' copper sensor plates to EVMs.
The target is a 4''x6'' copper plate, grounded to the EVM's ground. EVM is connected to desktop computer/laptop (plugged in) via USB cable.
For measurements I use the default (longest) integration times and lowest count rate.
Under these settings, the effective measurement range is 3 cm.
Problems:
1). fdc2214evm seems to be super sensitive to noise (even more than 1004EVM!)
If the shielding of my coax cables is floating or connected to IN0B, I pick up some stray interference, which causes my signal to drift away.
(Although in the link below it says that the best settings is connecting IN0A and IN0B)
The situation improves, if cable shielding is connected to the ground.
However, even in that case I still have interference pick up through the supplied USB cable!
Indeed, when i touch or at least bring my hand close to usb cable, the signal drifts away.
It should be noted that only channels connected to sensors with long cables are susceptible to this.
The signal from EVM board sensors is not affected by wiggling usb cable.
At the same time, when FDC1004evm is connected to computer with USB cable, I do not notice such effect.
Would you please advise if I'm doing it all correct and how to improve noise immunity?
2). With FDC1004evm I need to have the shielding of my coax cable connected to shielding of EVM board (not floating or grounded), otherwise it gets saturated with the cable (1.5 m).
It does not really matter what is select in gui settings for the active shielding - the result don't change much if it is disabled, set to follow the channel or used with CAPDAC,
as long as I coax shielding is connected to gui shielding.
Is it how it is supposed to be?
3). I noticed that they my noise gets higher when I bring my hand close to the EVM (both 2214 and 1004).
Also, currently my setup is sitting on the metal cart and I can see a signal drift on both EVM if I touch the cart.
Would you please advice how to shield EMV boards themselves?
4). Finally, a more general question. I need to detect position changes of a conducting target (human).
Do capacitive sensors outperform inductive ones (TIDA family) in these applications?
If yes, would you please kindly suggest an appropriate EVM?!)
Thank you in advance for your help)
Sincerely,
Alex