Other Parts Discussed in Thread: DAC3484, DAC3482
hi all,
After reading the datasheet of DAC3484, I have several questions:
1. If the mixers are disabled, can it be used as normal DAC with 4 independent channels?
2. If it is used in dual channel mode, according to the datasheet, only channel B and C are active. The parallel data interface will become same as DAC3482? That is, only data for channel B and C are interleaved at rising falling edge of the dac clock, and no need for channel A and D data. Is that so?
best regards
Xiang Chao