Part Number: FDC1004EVM
Other Parts Discussed in Thread: FDC1004, , MSP430F5528, MSP430F5529, ENERGIA, MSP-EXP430F5529LP
Hello there,
I am trying to read the capacitance of basic parallel plate capacitor, the capacitance between ground plate and sensor plate. It is actually a micro-structure and the gap between the ground and sensor plates changes. And this capacitive sensor is connected to FDC1004 EVM by about 1 m long coaxial cable. There are two major issues with my sensor application. Hope you give me great comments.
1) How to remove or minimize parasitic capacitance appearing in a dynamic environment? For example, when my finger touches the coaxial cable connecting the EVM and my sensor, the capacitance read by the FDC1004 EVM is changed.
2) Is it available to collect all the data points mentioned in the company datasheets (400 samples/s, 200 samples/s, and 100 samples/s)? I realized that the software working with FDC1004 EVM does not take all of the data., for example by the 400 samples/s mode, it collects only about 60 data points. Something it collects different number, not 60 points. If it is possible, how to collect all the data points?
It is said that if this firmware "Capacitive Sensing Sample Code (Energia) v1.1 (Rev. A)" is written to the FDC1004EVM, it is available. And it must be compiled and can then be uploaded to an MSP430. However, it is a little bit hard to catch up.
Can it the code "Capacitive Sensing Sample Code (Energia) v1.1 (Rev. A)" be written to the FDC1004EVM through the GUI software, for the FDC1004EVM is composed of I2C converter based on MSP430F5528 micro-controller and FDC1004? It seems that the company website does not provide a user guide for the code.
Can you give me your comments about my questions? Your comments will be great. Thanks.
TB