Part Number: DAC2904
Hi ,
We are using DAC2904 in one of our carrier board and we are connecting same BUS for both the channels as shown in the attached image. The length matching details also attached herewith. In the SOM we are using length difference is more than 1.5 inch is there between the signals . My question is what is the maximum tolerance we can have between the signals for DAC2904? Length difference of 1.5inch is acceptable?