Hello,
I have a question regarding the offset and gain error in case of DACs, as I am a rookie on the subject. I saw that many datasheets indiacate the gain error as +/-x% and I am wondering if the actual value could go above FSR, in case the DAC is supplied from a higher voltage than FSR, or this means that as the slope is steeper than the ideal one it will touch the FSR value sooner and will saturate at that value for the next upcomming codes.
Also for the offset error I observed +/-1LSB and I am wondering if -1LSB means that if I apply 1 to the input I get 0 on the output (and also if I apply 0 to the input the output is still 0) and +1LSB means that if I apply 0 I get 1 on the output (following the same approach a -1 will generate a 0 to the output, in case of sw calibration)?
Thank you very much for your support!
Florin