Part Number: ADC32RF45EVM
I have set the capture window as 65536 and analysis window as 4096 ( continuous capture off) while capturing two channel data from ADC32RF45EVM using a TSW14J56EVM. In this case when I press the capture button the FFT displayed is a 4096 point FFT. But there are 16 blocks of 4096 samples in the 65536 block of data captured. So is the 4096 point FFT that is displayed on the screen an average of all the 4096 point FFTs from the block of 65536 samples? This is not clear from the GUI user guide.
Same question regarding the case when continuous capture is ON.