Part Number: ADS1232REF
Hi There,
I have purchased four ADS1232REF units and have problem with one of them in assigning the calibration weight in scale mode configuration.
It is currently stock in negative weight in -xx.KG format where the other units accept in xx.xKG. format.
Using the switches for changing the digits doesn't help to get rid of the negative sign and bring the calibration weight back to the positive values.
I have tried resetting the unit using the RESET button, thinking that it will reset to the factory settings; but doesn't.
Please help me with correcting this problem.
Also the maximum value for the calibration weight is 99.9KG and I'm using load cells of 1000KG capacity. I had to redefined the units of measurements as 99.9KG entered value for calibration weight is actually representing 999KG and then, multiply the displayed values by factor of 10 to measure the correct load readings in KG units.
I have got around this limitation, however, I wonder if there is a way of changing the calibration weight limit in the unit's config mode or firmware beyond the default top limit of 99.9KG.
The units I'm using are V 1.2.0.