Part Number: TSW1400EVM
Other Parts Discussed in Thread: AWR1642BOOST
I am trying to read the Raw ADC data using the following setup and tutorial "training.ti.com/mmwave-sensor-raw-data-capture-using-tsw1400-board".
AWR1642Boost, MMWAVE-DevPack, TSW1400EVM.
When I connect the boards, power them on and open the HSDC pro, I do not have the same ADCs available in the list as compared to the tutorial.
My HSDC Version is: 4.9
The version used in the tutorial is 4.7.
Should I install that version?
Or can I use any of the available ADCs in my HSDC pro? In this case, kindly recommend the ADC which I should use with the mentioned setup?
Many Thanks.