I've downloaded the latest PLABS-SAR-EVM-PDK software, running on 64-bit Windows 8.1. Unfortunately, when the software comes up I am not able to resize the window so I can access the PSI controls along the bottom of the window. Clicking the little square in the upper right corner will not fit the window to my screen, nor am I able to grab the edge of the window and drag it diagonally to reduce the window's size. Do I have a Windows driver problem? What do I need to do to fit the SAR EVM window to my monitor so I can access all the controls?