Part Number: AFE4404
Hello,
I have been working with an AFE4404 + SFH7050 sensor and everything seems to work. I control them with an Arduino and have been able to get CLKOUT and output led values from AFE. However, other register values always return zero even after I enable REG_READ.
I need to know these information:
- in an i2c operation before reading a specific register (e,g, reg 0x23), should I do a write i2c_write(0x00, 0x01) to enable reading, then maybe wait for some time, and then do a write to target register followed by requesting 3 bytes? I did exactly this and just received zero.
- should I skip sending a start flag on i2c bus and write the target register after writing REG_READ? I haven't tried it.
- REG_READ will stay enabled and requires being set only once or I will need to do the operation every time I want to read a register?
Thanks,
Mona