I am looking for a DAC for my new design with inbuilt EEPROM or Flash to retain DAC configuration during power on and produce set Voltage. Output voltage upto 15V.
Please suggest
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for a DAC for my new design with inbuilt EEPROM or Flash to retain DAC configuration during power on and produce set Voltage. Output voltage upto 15V.
Please suggest
Hi Kevin,
This DAC is to provide Excitation to Pressure Sensors.
--> Minimum Excitation Required 12.5V at Sensor end. (Looking for 15V DAC bkz if any cable loss, it is to be compensated)
--> Steps : 100mV with +/- 1mV accuracy.
--> Resolution : Min. 8 Bit (10/12/16 is better)
--> Line Regulation ≤ 0.03%
--> Load Regulation ≤ 0.01% of set voltage
--> Stability over Time (8 Hrs) ≤ 0.01% of set voltage
--> Stability over temperature ≥ 50ppm/Deg C
--> Ripple ≤ 0.2mVrms
Looking for a DAC with non volatile register/EEPROM/Flash so that it can retain set voltage. Once the required voltage is set, the DAC should generate the voltage every-time it is powered up. Excitation voltage is changed whenever sensor is changed or calibration is done.
--
Regards,
Ramakrishna D C