Part Number: DDC1128EVM
Hi guys,
So I am trying to write a python code to fetch the data from DDC1128EVM board.
I have made some progress with fecthingthe data but there are some issues in it!
I have 192 buffer full with data not all 256. No idea why!!
Also when I try to configure the DDC register, I am not able to fetch data from DDC. I get a negative return value from the function.
To summarise: I am able to fetch data when i do not configure DDC register or FPGA code. Either of them or together!
I am attaching my code so you guys can also have a look at my code. I tried to make the code readable!!
I hope to have a good discussion over it!
Thanks & regards,
KushalFast_data.zip