This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer Qunling is working on a project. In this project, they get four signal need to be sampled, one high speed signal, grid current、voltage、one slow dc signal. And the high speed signal need to have 5us time resolution, so we recommend ADS8861, which is 1MHz ADC. And for the left three signal, they need sample at same time, so we recommend ADS131E04, which has 4 ADC inside, could do simultaneous sampling.
Now they need to synchronize those two ADC together. This means that they want to know the four signal value at the same time, and they need to display them. And according to your rich experience, do you get a way to achieve this? And for the signal measure, do you have any better solution or parts to achieve this?
Thanks and Best Regards,
Will
Hello Will,
Thanks for your post!
There are a couple of things to consider here.
Typically one of the best ways to synchronize multiple devices is to use the same clock source. This is an issue for the proposed design since the ADS8861 only uses an internal clock and there is no option (that I am aware of, I support Delta Sigma architecture devices) to output the internal clock of the ADS8861 to the ADS131E04.
Additionally, the delay for the data output of the ADS131E04 will be much greater than that of the ADS8861.
Are they hoping to measure transients using the ADS8861? Is this for protection purposes or only diagnostics?
Using a 4ch simultaneously sampling SAR or 4 1ch SAR's may be a more viable approach here depending on what the customer is trying to accomplish.
Hi Alex,
Thanks for your reply.
Actually the high speed signal is a PWM signal, they want to detect the slope, and the rise time and fall time error need to lower than 5us, so 1Msps data converter is preferred. And as far as I know, we don't offer one part that has 4 channel 1Msps simultaneously sampling SAR adc, am I right?
Thanks and Best Regards,
Will
Hi Alex,
Appreciate your help. And looking forward hear from Luis.
Best Regards,
Will