This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF80: ADC input reference circuit

Part Number: ADC32RF80

Hello,

1. Do we have a reference circuit by using NCS1-422+ for ADC analog input?

   If yes, please provide it. If no, it would be helpful if the recommendation circuit is provided.

2. We are seeing TCW1-3901+. Which NCS1-422+ or TCW1-3901+ is recommended?

The target RF frequency is 3400 to 3600MHz.

Best regards,

Toshihiro Watanabe