This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84: NCO only config: output attenuates with frequency

Part Number: DAC38J84


Hi,

I am using DAC38J84 EVM. Its setup for NCO only config, DAC input is set to 1GHz

input is constant, and DAC CLK is 10MHz. PLL is locked. 

following are p2p value at differetn frequencies.

40mV p2p at 200MHz. 100mv p2p at 100MHz, 250mV p2p at 10MHz.

is this behavior expected?

config values are attached. termination is 50 ohms.dac_config.cfg

Regards,

Anjana