This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/PGA970: ARM 5.2.9 compile failure

Tool/software: TI C/C++ Compiler

Hello, I recently installed ARM compiler 5.2.9 and have had a two errors for the object file of every module in the reference firmware. I need to get this thing working very soon, any help would be appreciated!

  • Hello,

    Can you please post the errors?
  • All is well now, I'm not sure how the make file executes it's build, but after doing the clean a couple more times the project finally compiled with no errors. It seems as if the object files from version 18 of the ARM compiler were still left in the build path after I switched over to 5.2.9

    But, on another topic, I am assuming that if I would want to get Vout fed into the A/D port of another controller then I will need to solder a test lead to the amplifier out side of C12 on the eval board? I would prefer to pin off of the Vout test point, but that test point is still in the feedback path of the amplifier.