Part Number: ADS54J60EVM
Other Parts Discussed in Thread: ADS54J60,
Hello,
I recently purchased boards ADS54J60EVM and TSW14J56EVM. I am following the SLAU629A user guide to configure my capture. I have installed all the software without problems. I have two separate 5V ,3A power supplies supplying the board. I encounter two errors on steps 2.3.2 HSDC PRO GUI Configuration. In this step, i choose the ADC from the drop down menu. I choose the ADS54J60_LMF_8224. When the firmware is updated, it takes 30 seconds and i see a increase in current.When i enter 983.04M in the ADC Output Data Rate, i encounter my first error.
then reset the board and try to capture. It returns this error.
when i checked the TSW Board. D3 is on and D8 is on. All other Lights are off. On the ASD board, the D2 PLL lock is on. All jumpers are on default settings. I disconnected all my connections and tried to repeat the procedures. I still get the same error messages.
Any help is appreciated. Thank you for your time.