Part Number: TSW1400EVM
Other Parts Discussed in Thread: ADS5294
Hi...
I am using TSW1400EVM to read the ADC Data.
I just want to know how to
1) Select the Device using MATLAB
2) Select the ADC using MATLAB.
When we open HSDC pro, the first option we get is to select the device. The device name is displayed in a pop-up screen, and we just want to click OK.
The next step is to select the ADC for which, we go to the menu in top left and select the ADC we want to use.
I just want to perform these two steps using MATLAB. What would be the commands that can help me do these? Secondly, do I need to write a command for Firmware as well? In HSDC pro, I don't select the firmware manually. While installation and patch, the firmware .rbf file was placed in the specific folder. So I hope I do not need to write a MATLAB command or firmware explicitly.
Thanks in advance