Part Number: DAC38J82EVM
Other Parts Discussed in Thread: DAC38J82
38J82: LMFS:8 2 1 2 HD :1
channal A can ouput data but channal C can not ;
why channal C can not out put data;
Please help me solve this problem;
Thank you ! best wishes
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC38J82EVM
Other Parts Discussed in Thread: DAC38J82
38J82: LMFS:8 2 1 2 HD :1
channal A can ouput data but channal C can not ;
why channal C can not out put data;
Please help me solve this problem;
Thank you ! best wishes
User,
This DAC can output 2 paths on any of the four available outputs. Is there a chance you have the part configured for CHB or CHD as the second output? The TI GUI sets the DAC38J82EVM to use CHA and CHB by default. For CHA and CHC operation, make sure the following two addresses are set as follows:
ADD Data
0x22 0x1B27
0x1A 0x0025
This sets the output mux to send data to CHA and CHC. This also sleeps CHB and CHD.
Regards,
Jim
I tried this configuration, but there is still no output.
Must the FPGA's lane ID match the ID of the DAC38J82?
I have a new trouble now.
I configured the DAC LMFKS 821 20 1 FPGA clock:100M, DAC Output rate 800MSPS
Channal A default output is 50M,If I want the output of 70, do I need to modify the NCO register?
How to modify some registers of NCO? Is there an example?
Thank you !