This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300EVM-PDK: AFE4300 Device GUI and Labview 2010?

Part Number: AFE4300EVM-PDK
Other Parts Discussed in Thread: AFE4300

I tried unsuccessfully to install AFE4300 Device GUI, but as I already have Labview 2010 installed, the GUI does not run because it seems to use an older Labview version? What should I do? Are the VI files for the Device GUI  available so that I can load it into Labview 2010 ?

  • Hi Lester,

    Let me check with the team and get back to you.
    However we can't provide the the VIs as it has other sensitive information in it.

    Regards,
    Prabin
  • Hi Lester,

    We would need following information to find the root cause of the issue.

    1) Screenshot of the error you are facing when installing the GUI and launching the GUI.
    2) Screenshot of the “National Instruments Software” in control panel
    a. Open Control Panel -> Programs and Features
    b. Double Click “National Instruments Software” and take a screenshot of the window

    Regards,
    Prabin