Part Number: AMC7891
Other Parts Discussed in Thread: TPS7A91, DAC6311, DAC7311, TINA-TI, DAC5311
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
TI have any Evaluation board with voltage regulators .Feedback controlled by DAC. Like below link
e2e.ti.com/.../how-to-build-a-monitor-and-control-solution-for-voltage-regulators
Hi,
TPS7A91 EVM used resistors for changing output.But how to proceed with DAC .and ADC to connect at output of LDO? kindly clarify.
Regards
var
Hi Vara,
This article explains the calculations to determine the three resistor values for the circuit.
The LMP would be connected in a similar fashion as below. If the VOUT range you desire is greater than the ADC input range of the LMP, then you should use two resistor resistors to create a divider to scale the VOUT to a lower value. I is also recommended that you have a 10nF capacitor on the input of the ADC if you are using the resistors to scale the input.
Thanks!
Paul
Regulator margining.TSCYou can also take a look at this TINA-TI simulation if you would like.
Thanks!
hi paul,
Thank you very much.Shall we get for for ADC also like these type of article with DC-DC converter.
Regards
Var