Hello,TI Experts,
I am now using afe5805,
Now I'd like to change PGA through SPI interface~
But I failed,do I need to enable anything to change PGA successfully?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Fawn,
Can you confirm if you have written the initial commands through the AFE5805 GUI?
This step is used to adjust ADC input and output configuration. Therefore, TSW1400 can correctly capture data.
1. Set Address Byte(s) = 0 Data Byte(s) = 1. Click any space area to send command to AFE5805.
2. Set Address Byte(s) = 42 Data Byte(s) = 8081. Click any space area.
3. Set Address Byte(s) = 46 Data Byte(s) = 8208. Click any space area.
If you have already done the above, can you provide more details as to what happens when you change the PGA settings in the GUI?
Some screenshots of the error message (if any) will help.
Hi Fawn,
First we will need to check if the SPI is working fine.
Can you enable the powerdown mode and check if the supply current is reduced?
Since you do not have the data capture card TSW1400EVM, how do you verify the ADC data from the AFE5805EVM?