Other Parts Discussed in Thread: ADS1247, ADS1248
Hello, I recently purchased a few ADS1246 to accurately measure the voltage on a laser diode thermistor. I am using an Arduino Uno to interface with the chip and am using a power supply at 1.25V and a 2.048V external reference to test the chip. I am not able to communicate with the chip and do not receive any data ready signal. I saw in the datasheet it mentions that the SCLK needs to be a multiple of eight but it also says later that the minimum SCLK period corresponds to a frequency of no more than 2MHz. The Arduino Uno's pre-scaler does not allow for it to generate any frequency below that that is a multiple of eight. I am just wondering if I am doing something wrong or if this chip is incompatible with the Arduino Uno. If this is the case what microcontrollers are recommended for use with this product?