Part Number: DDC1128
Dear Specialists,
My customer is confirming DDC1128EVM and has a question.
I would be gtateful if you could advise.
---
I got the data from DDC1128 Firmware by using (Data tab/Save Data From Memory).
Regarding obtained data, I have no idea of what it is.
Could you explain what it is.
For example, the first line is 256A,0.000000000,16748760.000000000,0,4.096000000,16.
What do they represent each?
Especially 16748760, I think it's an output conversion data.
Is it binary, octal, hex or decimal?
I think decimal, is it correct?
Also this data is quite large value,
I presume the addition seems to be done so that the upper 8 bits of 24 bits all become 1 on the original 16bit data, and then change to decimal.
Is this recognition correct?
I'd also like to know what other data is.
Could you send an application manual, EVM manual is not enough.
8204.with AIB_0R1VINPUT_700μsec_Range0_16bit.txt
I would like you to respond as soon as possible.
If we do not know this we can not proceed with the consideration.
---
I appreciate your great help in advance.
Best regards,
Shinichi