Other Parts Discussed in Thread: , LMK04828, LMK04616EVM, LMK04616
Hello,
I use ADS54J60EVM with TSW14J56 in order to decide the optimal conditions to operate the ADC.
I followed the instructions in slau629i and managed to receive successfully digital samples in HSDC GUI @ 983.04 MSPS with SFDR = 90 dBFS.
Then, I tried to change the ADC sample rate to different value using the following steps:
- Loading the “LMK_Config_Onboard_409p6_MSPS.cfg” file, verifying D2 is lit, pressing SW1 to reset the ADC, loading the “ADS54J60_LMF_4244.cfg” file.
-
Opening the HSDC GUI and select in ADC drop-down menu the “ADS54J60_LMF_4244” option, set the “ADC Output data rate” to 409.6M and reset the board.
As before, I received the digital samples, however, now the FFT contains much more spurs and the SFDR decreased dramatically to 45 dBFS.
I repeat the steps above for 819.2 MSPS, and the spurs are still exist. However, setting the sample rate to 491.52 MSPS yields to SFDR ~ 90 dBFS.
My questions are:
-
Are the steps mentioned above correct?
-
If so, why is there such a significant difference between the results?
-
What is the right way to configure the ADC to operate in 409.6 / 819.2 MSPS without all those spurs?
Thanks in advance,