Part Number: DAC1282
I have been having an issue with the SPI interface on the DAC1282.
After some testing, it appears that the tRSTM (PWDN/RESET high to begin operation) timing parameter in the datasheet is incorrect. While I haven't fine tuned my code as yet, by observing the output of the DAC when it powers up, I suspect that this parameter is closer to 20msec, not 500nsec as shown in the datasheet.
Can someone confirm if this parameter is the same length as the power-on reset parameter, which is 2^16 fCLK periods?
Thanks,