I am looking for a power supervisor (3.3VDC CPU), watchdog (Windowed WDOG) IC with a /RESET output for the uC that also contains a RESET that can be used by the CLR pin of the DAC7750 IC. I prefer not to use an inverter to create a RESET from a /RESET. I believe I've seen these in the past, however cannot seem to navigate in the website sufficiently to locate them now.