This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1198: ADS1198

Part Number: ADS1198

Hi - I am trying to understand the operation of the ADS1198 when driven by a single ended input voltage. I have the ADS1198 eval board and the EVM software. The channel is set to normal electrode and PGA gain = 1. If I connect INN input to 0V and drive INP to 1V should I read 1V? The ADS1198 EVM software is giving scaled results. For example if AVDD = 3V, Vref=2.4V and Vin=1V the read voltage is 1.7V, and if Vin=1.2V the read voltage is 2.05V. In another example if AVDD = 3V, Vref=4V and Vin=1V the read voltage is 2.3V, and if Vin=1.2V the read voltage is 2.76V.  In another example if AVDD = 3.3V, Vref=3.3V and Vin=1V the read voltage is 2.07V, and if Vin=1.2V the read voltage is 2.5V. What is causing the scaling? 

Thanks,

Diarmuid.

  • Hello Diarmuid,

    Thank you for your post and welcome to our forum!

    What is AVSS connected to? I assume you are using a unipolar supply with AVSS = GND?

    The ADC will convert the differential input voltage between INP and INN. In principle, if INP = 1 V and INN = 0 V, the ADC output should read 1 V. However, there is another restriction on the input voltage due to the internal PGA: the input common-mode voltage. The PGA amplifiers are not able to swing to the rail, so the input common-mode must be kept at least 200 mV away from each supply rail.

    Try increasing INN to mid-supply (1.5 V) and connect INP to 2.5 V.

    Best Regards,

  • Hi Ryan, 

    Thanks for the reply. Yes AVSS = 0V. I have run a number of tests to try to isolate the problem. When I set INN=1.5V and INP=2.5V I do indeed get Vout=1V. I ran two tests with INN=1.5V and INN=1.2V, and ran the tests at both VREFP=2.4V and 4V. Below are plots showing Vout against the differential input voltage, so for the case of INN=1.5V INP was swept from 1V to 2.5V in 0.1V steps. As can seen seen when VREFP=2.4V there is a good agreement between the differential voltage and Vout. However when VREFP=4V Vout is scaled by about 1.34. This is close to the ratio of VREFP/AVDD (4V/3V) could this have a bearing on the result? 

    I also done tests with INN=0V and swept INP from 0V to 1V in 0.1V steps. Again the results below show the same scaling when VREFP=4V. 

    I have run additional tests and made both AVDD and VREFP=3.3V on the eval board but I the scaling effect does not go away - in fact it gets worse.

    Any help appreciated.

    Diarmuid 

    ADCTestData.pdf

  • Hello Diarmuid,

    Apologies for not noticing this in your first post. When AVDD = 3 V or 3.3 V and AVSS = 0 V, you cannot use the VREF = 4 V setting. Essentially, the output of the reference buffer (Figure 26) is railing and unable to reach 4 V. If you probe the VREFP pin with respect to AVSS, you should see that the reference voltage is less than 4 V. The ratio of VREFP to "4 V" is likely the dominant source of the gain error in your plots for VREF = 4 V.

    Please review the External Reference section of the Electrical Characteristics table.


    Best Regards,

  • Hi Ryan,

    Many thanks again for your reply. Yep when I make AVDD=3V and set VREFP=4V the measured VREFP=2.96V. Also, if I make AVDD=3.3V and set VREFP=4V the measured VREFP=3.24V. However when I power down the internal reference and use an external reference results are a little confusing. If I make AVDD=3.3V VREFP=3V and set INN to some midscale voltage (e.g. 1V or 1.5V) again I get a scaling issue at the output.

    Also, at times the eval software can give erratic results - repeated voltage sweeps give differing output voltage readings. I am not sure if this is an issue with the software or the hardware. 

    Regards,

    Diarmuid.Figure 1 AVDD.pdf 

  • ADS1198FrontendTest.pdfHi Ryan,

    To get a better understanding on the ADC I have added a LDO regulator to provide a mid-scale reference voltage for INN and adjusted the PGA gain and re-run the INP sweep tests. Attached are the results - again I am seeing a 200mV offset in the readings. I want to use channel 1-8 as ADC inputs (without any ECG functionality) - I have turned off all WCT, RLD and pace functionality is there anything else in the setting that could cause the offset?

    Thanks,

    Diarmuid.  

  • Hi Diarmuid,

    What power and reference settings were you using for the last test?

    The output being limited to lower voltages as the gain increases is expected since the full-scale range of the ADC remains the same.