Part Number: ADS5400
I am trying to determine the maximum allowed clock input signal to an unpowered ADS5400. In other words, can a differential clock be applied prior to power on?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS5400
I am trying to determine the maximum allowed clock input signal to an unpowered ADS5400. In other words, can a differential clock be applied prior to power on?
The absolute maximum specifications do not address power off and do not make sense relative to a power off condition. For example, the specification states that the minimum of the clocks to gnd is 0.5 to 4.5. Obviously, with the device off and nothing driving it, this cannot be met. Most of the time, these specifications are written w.r.t. VDD itself. In the A/Ds case, they assume power is applied and within certain limits.
Then there is the second requirement of the voltage DC between the two clock pins must be a minimum of 2V and maximum of 3V. I do not understand this one at all. The clock signals is driven with an AC coupled balun. I would expect 0V DC between the pins.
CLKINP, CLKINN to GND(2) Voltage difference between pin and ground 0.5 4.5 V
Voltage difference Continuous AC signal 1.1 3.9 V
CLKINP to CLKINN(2) between pins, common
mode at AVDD5/2 Continuous DC signal 2 3 V
Charles