Hi,
I am using ADS58J63 in my design. I was planning to do ground separation for Analog and Digital signal lines. I checked the EVM schematic and there no such separation is done. I see in the device pin diagram there are separate AGND and DGND pins. Regarding this I had couple of queries.
1. Are these pins separate internally also so that I can use separate grounds?
2. Or are these AGND and DGND pins are internally connected to same ground and hence separating them externally won't have any effect?
Regards,
Kiran